STM32L433: Low level driver and Comparator startup time
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-16 6:19 AM
Hallo. I'm working in a STM32L433 and I'm using CubeMX tool to generate the initialization code.
I have a question regarding the comparators' Low level driver.Although I'm using both comparator input pin (In+ and In-) connected to external port, and so I don't use the internal voltage reference, the low level driver keep the time wait for voltage scaler stabilization, but the internal voltage reference is off and the 'SCALEN' bit in 'COMP1_CSR' register is set to 0.This is a low power application so I have should return in standby mode as quickly as I can, so I shouldn't wait this startup time if it weren't neccessary.Am I doing something wrong or it is a kind of bug in low level driver? Is there any configuration to inform CubeMX to not add the wait cycle?
How can I bypass the issue and, eventually, how can I give feedbak about this bug (If it were).Sorry for my english and thank you in advance.PaoloThis is the generated code block:
void MX_COMP1_Init(void)
{...cut...
/* Wait loop initialization and execution */
/* Note: Variable divided by 2 to compensate partially CPU processing cycles */ __IO uint32_t wait_loop_index = 0; wait_loop_index = (LL_COMP_DELAY_VOLTAGE_SCALER_STAB_US * (SystemCoreClock / (1000000 * 2))); while(wait_loop_index != 0) { wait_loop_index--; } LL_EXTI_DisableEvent_0_31(LL_EXTI_LINE_21);LL_EXTI_DisableIT_0_31(LL_EXTI_LINE_21);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-30 6:40 AM
Hi
paolo.andreuzza
‌,Thanks for sharing your case.
I will report the error to our CubeMX team who should make a deeper analysis and provide the needed fix for generated code in coming versions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-01 12:52 AM
Many thanks, Amel.
It's great to see a company actively monitoring their forums for issues and suggestions.Paolo