cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KBUx can't load program

Anthony Plantin
Associate
Posted on April 19, 2017 at 12:00

Hi there ,

We using AC6 IDE to develop our application based on VL53L0X and STM32L432KBUx. Everything was good until I can't program my target.

At the beginning only the debug session worked fine. But now I'm not able to start a debug sesions. I used stlink-utility to checked if the MCU was in write protection or something. With the stlink-utility I'm able to program and verifiy the MCU's flash. But the program doesn't run. And the MCU core is hatled and I can't run it.

I checked the reset line and everything is ok to me. The line is high and is driven by the stlink.

I Attached the error message from eclipse and the console error from eclipse as well.

Thank you for you reply.

Anthony

0 REPLIES 0