2018-04-26 10:04 AM
Hello All,
I am using STM32L486RGT, CubeMX 4.25 STM32L4 lib 1.11.
At the STM32 I have a 16MHz crystall connected.
Now I run into problems setting up the clocktree. It works under certain combinations but not under the ones I want.
I want to use the 16MHz crystal, HSE, PLL, USB and CPU running at 64MHz.
not working: 16MHz Crystal, PLLSource:HSE, PLLM:1, PLLN:8, PLLR:2, Sysclock:64MHz, PLLSAI1N:12, PLLSAI1Q:4, USB:PLLSAI1Q:48MHz
working: switching the PLL source to HSI
I tried also with Nucleo Board STM32L452 and found the combination does initially does not work.
I put an 16MHz crystal to the board.
working: 16MHz Crystal, PLLSource:HSE, PLLM:1, PLLN:8, PLLR:2, Sysclock:64MHz
not working: as above, plus USB, PLLSAI1N:2, PLLSAI1Q:4, USB:PLLSAI1Q:48MHz
On all examples: AHBPrescalers are 1 so all peripheral/core/sysclock clocks are 64MHz
Here is the example SysClock Init from the generated not working sample:
the failing function is:
<<
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
>>
Can anyone confirm those problems?
Regards, Adib.
--
/**
* @brief System Clock Configuration * @retval None */void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit;/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLN = 8; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{ _Error_Handler(__FILE__, __LINE__); }PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART3
|RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_I2C1 |RCC_PERIPHCLK_USB|RCC_PERIPHCLK_ADC; PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2; PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1; PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1; PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1; PeriphClkInit.AdcClockSelection = RCC_ADCCLKSOURCE_SYSCLK; PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLLSAI1; PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSE; PeriphClkInit.PLLSAI1.PLLSAI1M = 1; PeriphClkInit.PLLSAI1.PLLSAI1N = 12; PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV7; PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV4; PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV8; PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the main internal regulator output voltage
*/ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }/**Configure the Systick interrupt time
*/ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick
*/ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}2018-04-26 10:11 AM
Helloadib,
It could be that you faced CubeMX issue with code generation for clock domain.Could you please take a look on this thread:
https://community.st.com/0D50X00009Xkb5hSAB
? The issue described there is wrong PLLM parameter set by CubeMX.
Regards
Szymon
2018-04-26 12:32 PM
Hello Szymon,
indeed the PLLM was undefined :(
But even fixing this I run into timeout after setting the PLL parameter.
Any idea?
I have following values:
PLLSource 3
PLLM 1
PLLN 8
PLLP 7
PLLQ 2
PLLR 2
regards, Adib.
---
/* Configure the main PLL clock source, multiplication and division factors. */
__HAL_RCC_PLL_CONFIG(RCC_OscInitStruct->PLL.PLLSource, RCC_OscInitStruct->PLL.PLLM, RCC_OscInitStruct->PLL.PLLN, RCC_OscInitStruct->PLL.PLLP, RCC_OscInitStruct->PLL.PLLQ, RCC_OscInitStruct->PLL.PLLR);/* Enable the main PLL. */
__HAL_RCC_PLL_ENABLE();/* Enable PLL System Clock output. */
__HAL_RCC_PLLCLKOUT_ENABLE(RCC_PLL_SYSCLK);/* Get Start Tick*/
tickstart = HAL_GetTick();/* Wait till PLL is ready */
while(READ_BIT(RCC->CR, RCC_CR_PLLRDY) == RESET) { if((HAL_GetTick() - tickstart) > PLL_TIMEOUT_VALUE) { return HAL_TIMEOUT; } }2018-04-26 12:50 PM
Hello Szymon,
I tried further and used the LL driver for RCC initialisation.
This works, but somehow the systick interrupt was shut off.
So all the HALDelay did not work ...
I will investigate tomorrow.
(I can't await the fix in CubeMX)
Regards, Adib.
--
2018-04-26 12:57 PM
added:
LL_SYSTICK_EnableIT();
before running to while(1) {
and then it works.
Maybe an other problem on RCC_LL initialisation.
regards, Adib.
--
2018-05-29 4:31 AM
Hello ST Team,
I tried the cubeMX 4.25.1 with no luck on this project.
Although the releasenotes claimes the clocksettings has been fixed for STM32L4.
Please investigate.
Adib.
--
2018-05-29 6:02 AM
Hi Adib could you please share your ioc and give me some more details about the board you are using please
2018-05-29 6:39 AM
Hello
Taraben.Adib
,I will raise your issue internally for check.Can you please share your ioc file?
With Regards,
Imen.
2018-05-29 6:59 AM
Hi Imen, please could you guide me how to append files. I don't see any attach button :-? Thanks, Adib.
2018-05-29 7:07 AM
ok , found that. Editing the original post allows to attach files; uhmm 'not so intuitive ..'.
I use the sam2_goware.ioc using the LL driver.
When switching to HAL for RCC module I am stuck in ClockConfiguration.
HTH, Adib.