cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1xx SPL 1.2.0: Bug with IS_RCC_FLAG

Phil1
Associate II
Posted on July 03, 2014 at 10:52

Scenario:

Our product displays the Last Reset Reason (from the RCC) when it powers up. This allows us to determine if the last reset was intentional or caused by e.g. a power brownout or software failure. Problem: When USE_FULL_ASSERT is defined, RCC_GetFlagStatus() uses the IS_RCC_FLAG macro to determine whether the passed value is a valid RCC flag. Attempting to check the state of theRCC_FLAG_OBLRST RCC flag causes an assertion failure. Cause: The IS_RCC_FLAG() macro (stm32lxx_rcc.h) is incorrectly defined. RCC_FLAG_WWDGRST is checked twice, andRCC_FLAG_OBLRST is not checked at all:

1.
#define IS_RCC_FLAG(FLAG) (((FLAG) == RCC_FLAG_HSIRDY) || ((FLAG) == RCC_FLAG_HSERDY) || \
2.
((FLAG) == RCC_FLAG_MSIRDY) || ((FLAG) == RCC_FLAG_PLLRDY) || \
3.
((FLAG) == RCC_FLAG_LSERDY) || ((FLAG) == RCC_FLAG_LSIRDY) || \
4.
((FLAG) == RCC_FLAG_PINRST) || ((FLAG) == RCC_FLAG_PORRST) || \
5.
((FLAG) == RCC_FLAG_SFTRST) || ((FLAG) == RCC_FLAG_IWDGRST)|| \
6.
((FLAG) == RCC_FLAG_WWDGRST)|| ((FLAG) == RCC_FLAG_LPWRRST)|| \
7.
((FLAG) == RCC_FLAG_WWDGRST)|| ((FLAG) == RCC_FLAG_LSECSS))

Fix: The last line should be changed to:

1.
((FLAG) == RCC_FLAG_OBLRST) || ((FLAG) == RCC_FLAG_LSECSS))

This allows RCC_FLAG_OBLRST to be passsed as an RCC flag, and have its status checked without causing an assertion failure. #rcc_flag_oblrst-stm32l1xx-bug
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on July 03, 2014 at 12:58

Hi Phil Pemberton,

This defect is fixed in STM32L1xx Standard Peripherals Library V1.3.0 available here http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257913 

Thanks for the report.

With regards.