Question
STM32L15x TIM5 Internal Trigger (ITR)
Posted on February 18, 2014 at 03:18
In RM0038 Table 66 (page 379) the Internal trigger connections (ITR) has no entry for TIM5.
There's no text describing any functional differences for TIM5 over TIM[234] with respect to these ITR connections, nor does the StdPeriph library reject setting those values, nor does the device-specific . Does anyone know if there are any such connections? The following forum thread (for STM32F2xx)/ca09bc80
gives me hope that it is an omission. #stm32l1 #tim5 #trigger #tim