cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L152 Discovery I2C problem with status register

rdoljak
Associate
Posted on July 11, 2014 at 10:53

Hello 

My problem is that i cannot communicate with the temperature sensor via I2C because the code stop working and the problem is in the status register but i dont know how to fix it

can anybody can help me ?

this is the communication code:

#include <stm32l1xx.h>

#include <stm32l1xx_i2c.h>

// this slave address belongs to the STM32F4-Discovery board's

// CS43L22 Audio DAC

// connect PD4 to VDD in order to get the DAC out of reset and test the I2C

// interface

#define SLAVE_ADDRESS 0x40 // the slave address 

void I2C1_init(void){

GPIO_InitTypeDef GPIO_InitStruct;

I2C_InitTypeDef I2C_InitStruct;

// enable APB1 peripheral clock for I2C1

RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

// enable clock for SCL and SDA pins

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

/* setup SCL and SDA pins

* You can connect the I2C1 functions to two different

* pins:

* 1. SCL on PB6 or PB8

* 2. SDA on PB7 or PB9

*/

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; // we are going to use PB6 and PB7

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; // set pins to alternate function

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz; // set GPIO speed

GPIO_InitStruct.GPIO_OType = GPIO_OType_OD; // set output to open drain --> the line has to be only pulled low, not driven high

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP; // enable pull up resistors

GPIO_Init(GPIOB, &GPIO_InitStruct); // init GPIOB

// Connect I2C1 pins to AF

GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); // SCL

GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_I2C1); // SDA

// configure I2C1

I2C_InitStruct.I2C_ClockSpeed = 100000; // 100kHz

I2C_InitStruct.I2C_Mode = I2C_Mode_I2C; // I2C mode

I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2; // 50% duty cycle --> standard

I2C_InitStruct.I2C_OwnAddress1 = 0x00; // own address, not relevant in master mode

I2C_InitStruct.I2C_Ack = I2C_Ack_Disable; // disable acknowledge when reading (can be changed later on)

I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; // set address length to 7 bit addresses

I2C_Init(I2C1, &I2C_InitStruct); // init I2C1

// enable I2C1

I2C_Cmd(I2C1, ENABLE);

}

/* This function issues a start condition and

 * transmits the slave address + R/W bit

 *

 * Parameters:

 * I2Cx --> the I2C peripheral e.g. I2C1

 * address --> the 7 bit slave address

 * direction --> the transmission direction can be:

 * I2C_Direction_Tranmitter for Master transmitter mode

 * I2C_Direction_Receiver for Master receiver

 */

void I2C_start(I2C_TypeDef* I2Cx, uint8_t address, uint8_t direction){

// wait until I2C1 is not busy any more

while(I2C_GetFlagStatus(I2Cx, I2C_FLAG_BUSY));

// Send I2C1 START condition

I2C_GenerateSTART(I2Cx, ENABLE);

// wait for I2C1 EV5 --> Slave has acknowledged start condition

while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_MODE_SELECT));

// Send slave Address for write

I2C_Send7bitAddress(I2Cx, address, direction);

/* wait for I2Cx EV6, check if

* either Slave has acknowledged Master transmitter or

* Master receiver mode, depending on the transmission

* direction

*/

if(direction == I2C_Direction_Transmitter){

while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

}

else if(direction == I2C_Direction_Receiver){

while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED));

}

}

/* This function transmits one byte to the slave device

 * Parameters:

 * I2Cx --> the I2C peripheral e.g. I2C1

 * data --> the data byte to be transmitted

 */

void I2C_write(I2C_TypeDef* I2Cx, uint8_t data)

{

// wait for I2C1 EV8 --> last byte is still being transmitted (last byte in SR, buffer empty), next byte can already be written

while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_BYTE_TRANSMITTING));

I2C_SendData(I2Cx, data);

}

/* This function reads one byte from the slave device

 * and acknowledges the byte (requests another byte)

 */

uint8_t I2C_read_ack(I2C_TypeDef* I2Cx){

// enable acknowledge of received data

I2C_AcknowledgeConfig(I2Cx, ENABLE);

// wait until one byte has been received

while( !I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_BYTE_RECEIVED) );

// read data from I2C data register and return data byte

uint8_t data = I2C_ReceiveData(I2Cx);

return data;

}

/* This function reads one byte from the slave device

 * and doesn't acknowledge the received data

 * after that a STOP condition is transmitted

 */

uint8_t I2C_read_nack(I2C_TypeDef* I2Cx){

// disable acknowledge of received data

// nack also generates stop condition after last byte received

// see reference manual for more info

I2C_AcknowledgeConfig(I2Cx, DISABLE);

I2C_GenerateSTOP(I2Cx, ENABLE);

// wait until one byte has been received

while( !I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_BYTE_RECEIVED) );

// read data from I2C data register and return data byte

uint8_t data = I2C_ReceiveData(I2Cx);

return data;

}

/* This function issues a stop condition and therefore

 * releases the bus

 */

void I2C_stop(I2C_TypeDef* I2Cx){

// Send I2C1 STOP Condition after last byte has been transmitted

I2C_GenerateSTOP(I2Cx, ENABLE);

// wait for I2C1 EV8_2 --> byte has been transmitted

while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

}

int main(void){

I2C1_init(); // initialize I2C peripheral

uint8_t received_data;

I2C_start(I2C1, SLAVE_ADDRESS<<1, I2C_Direction_Transmitter); // start a transmission in Master transmitter mode

I2C_write(I2C1, 0x01); // write one byte to the slave

I2C_stop(I2C1); // stop the transmission

I2C_start(I2C1, SLAVE_ADDRESS<<1, I2C_Direction_Receiver); // start a transmission in Master receiver mode

received_data = I2C_read_nack(I2C1); // read one byte and don't request another byte, stop transmission

while(1);

return 0;
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0