cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151C8T6/STM32L151CBT6 about ISP

xwang.6
Associate III

Can STM32L151C8T6/STM32L151CBT6 download ISP with one click?

Can you provide a reference circuit diagram?

3 REPLIES 3
Javier1
Principal

what do you mean with "download ISP with one click"?

Are you referring to Flashing the firmware trough an ISP with one click?

we dont need to firmware by ourselves, lets talk
FBL
ST Employee

Hello @xwang.6​ 

Could you explain what do you mean with one click? Do you mean updating the firmware with ST-LINK?

It is recommended to consult the datasheet for the specific programming tool you are using for more information on how to connect it to the microcontroller depending on your hardware setup.

Note that these products are no longer recommended for new design. Only to support customers ongoing production.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


xwang.6
Associate III

0693W00000YAYc8QAH.png0693W00000YAYqMQAX.png Please refer to Figures 1 and 2,Use software FlyMcu to download the program to PCB via USB to serial port( STM32 USART1)