cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 split powering analog and digital

mmensch
Associate II
Posted on May 25, 2016 at 15:22

Hi,

though I know that ST recommends using the same supply for analog (VDDA, VSSA) and digital (VDD, VSS) there are reasons in my application that make me want an extra analog supply. (My STM32L151 does not have external Vref-pins)

What can happen and how can I help it? Two antiparallel schottky diodes between VDDA and VDD? Other things?

Any information and help ist welcome

Thanks

Martin

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mmensch
Associate II
Posted on June 07, 2016 at 16:54

Hi everybody

still need some help on this topic

Martin

Chris1
Senior III
Posted on June 09, 2016 at 20:36

I think that the requirement is really, ''A maximum difference of 300 mV between VDD and VDDA can be tolerated during power-up and operation.''

ST's guidance suggesting using the same supply for VDD and VDDA is confusing (what's the reason for having VDDA then?), perhaps they mean to say derived from a common source.