STM32F7 Discovery Benchmark project - adding OTG_FS_PowerSwitchOn toggling problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-06-09 8:44 AM
Posted on June 09, 2016 at 17:44
Hi everyone, i'm trying to start playing with STM32F7 Discovery board, taking as base the benchmark project and modifying it. i did the following modification in stm32f746g_discovery.c:
GPIO_InitTypeDef GPIO_Init_Structure; GPIO_Init_Structure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_Init_Structure.Pull = GPIO_NOPULL; GPIO_Init_Structure.Speed = GPIO_SPEED_HIGH; /*GPIO_Init_Structure.Alternate = GPIO_AF12_FMC;*/ /* GPIOD configuration */ GPIO_Init_Structure.Pin = GPIO_PIN_1 | GPIO_PIN_5; HAL_GPIO_Init(GPIOI, &GPIO_Init_Structure); in main, i added the following: if (BSP_PB_GetState(BUTTON_KEY)) { HAL_GPIO_WritePin(GPIOD,GPIO_PIN_5,GPIO_PIN_SET); } else { HAL_GPIO_WritePin(GPIOD,GPIO_PIN_5,GPIO_PIN_RESET); } i can see in the, debbuging sesion, GPIOD ODR pin 5 going up and down, but the physical pin (OTG_FS_PowerSwitchOn) remains up without toggling. any clue why is this? thanks in advance
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0