cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L100xx USART Smartcard Mode

Malin Chekurov
Associate
Posted on September 20, 2017 at 12:31

So recently I had to dig in and fix some code about the USART in SmartCard mode. Apparently each byte i send is echoed back at me, triggering the RXNE. My question is do I get the RXNE before the TC of the byte I just send or after that.

According to the user manual: 'Then, the FE flag is set with the RXNE at the end of the 1.5 stop bit.', that means in the  case of a smartcard with Guard Time of say 10 etus, I will get the TC after the guard time(user manual- 'TC is forced low during this time. When the guard time counter reaches the programmed value TC is asserted high.' ) and the RXNE must be set after the 1.5 stop bits which is before the TC.

I have run that many times and it seems completely random - sometimes RXNE is set before TC and sometimes after it.

Also the user manual doesn't say anything on the echoed bytes.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0