cancel
Showing results for 
Search instead for 
Did you mean: 

External interrupt react on rising edge only

jan siroky
Associate
Posted on September 20, 2017 at 15:29

Hi everybody.

I am playing with stm32f411 and external interrupts. I have trouble with interrupt calling in the moment i need. Could you please take a look at my issue?

Id like to call the interrupt by user button pc13. The pin pc13 is pulled up. When the button is pressed, the pin pc13 is connected to the ground (falling edge). But whatever i set on interrupt setting (falling edge/rising edge), the interrupt procedure is called only leaving the button ('unpressing' it) (rising edge). 

here i put the setting of the interrupt that i use. 

void ext_int_pc13_conf()

{

RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;                  // syscf clk enable

RCC->APB2RSTR |= RCC_APB2RSTR_SYSCFGRST;            

// syscf reset

RCC->APB2RSTR &= ~RCC_APB2RSTR_SYSCFGRST;

SYSCFG->EXTICR[3] = SYSCFG_EXTICR4_EXTI13_PC;       // pin set as a trigger of ext interrupt

EXTI->IMR

|

= EXTI_IMR_MR13;                                                 // interrupt masking

EXTI->RTSR

|

= EXTI_RTSR_TR13;                                            // interrupt trigger on rising edge

EXTI->RTSR

|

= EXTI_FTSR_TR13;                                            // 

interrupt trigger on fallingedge

NVIC->IP[EXTI15_10_IRQn] = 0x4;                                           // priority setting

NVIC_EnableIRQ(EXTI15_10_IRQn);                                        // interrupt enable

return;

}

Thx for any idea!

js

#pc13 #external-interrupts-button #stm32f411 #stm32f4xx #external-interrupt
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0