cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L072CZ. NVM programming example project crashes.

GEORGE SANDLER
Associate III

Project based on "01_NVMEraseProg" from the "STM32L0xx_Snippets_Package_V1.2.0" crashes.

Below is a source code to erase/write 100 flash pages. Code crashes 9 time out of 10.

int main(void)

{  

 uint32_t addr;

 error = 0;

 SysTick_Config(2000); /* 1ms config */

 SystemClock_Config();

 ConfigureGPIO();

 if (error != 0)

 {

  while(1) /* endless loop */

  {

  }

 }

 SysTick_Config(16000); /* 1ms config */

  

 UnlockPELOCK();

 UnlockPRGLOCK();  

 for (uint32_t i=0; i < 100; i++)

 {

  addr = FLASH_USER_START_ADDR + (i * FLASH_PAGE_SIZE * 4); // FLASH_PAGE_SIZE is in words

  FlashErase(addr);

  FlashHalfPageProg(addr, data_for_hpage);

  FlashHalfPageProg(addr + FLASH_PAGE_SIZE * 2, data_for_hpage);

 }

 LockNVM();

 while (1) /* Infinite loop */

 {

 }

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0