2016-06-22 05:17 PM
When I connect my board to my computer via usb (cn2) I lose the programming. I lost the factory programming to start with. I downloaded the Keil uVision5 compiler and downloaded the blinky app to the discovery board. It works until I either unplug the usb cable and plug it back in or shut my computer off and reboot. Has anybody else had this problem? If I program my board and unplug the usb cable and plug it into CN3 (USB User) it runs properly.
Tom #lost-programming2016-06-22 05:21 PM
Has anybody else had this problem?
No, can't say I've heard anyone either. What version of firmware is running on the ST-LINK? Is it current?2016-06-23 06:25 AM
How do I find the firmware version?
2016-06-23 08:03 AM
Hi smuts.tom,
I recommend you to upgrade the ST-Link firmware version to V2-1 through this -Hannibal-2016-06-23 08:23 AM
How do I find the firmware version?
Well there is the debugger configuration pane in Keil, or you could use the ST-LINK Utilities.2016-06-23 06:34 PM
I have version 2-1 installed. I need to know whether it's my computer or the Discovery board so I ordered another board. I'll know Monday which it is.
2016-06-23 11:48 PM
The firmware version is something else, and can be updated to the current release via the ST-LINK Utilities.
2016-06-25 06:48 AM
OK. I just upgraded to V2.J27.M15 via ST-LinkUpgrade.exe