2017-10-31 02:17 AM
Hey
is there a way to use an USB drive to update the firmware of a STM32L053.
I know that DFU is a possibility, but I want to place the bin file on the stick, pressing the button at startup (or something like that).
Has someone an example of this ? (I think there is one for the F4 series)
2017-10-31 02:32 AM
The USB in 'L0 is device only, thus the answer is no.
JW