2015-08-03 11:20 AM
Hello !
We are working in a project that needs a glass lcd display, the average consumption of the system (MCU + LCD) must be around 50 uA. I always used a msp430 with integrated lcd controller to handle this kind of problems. But now I am very tempted to use a STM32L051R mainly due to the costs and performance. Anyone here already tried this? I read the AN2656 and noticed that is possible to interface a glass lcd with the stm32. But the average consumption in this application note was too high.2015-08-03 11:48 AM
Save time and money, using the more expensive STM32L053R.
That MCU has builtin LCD driver . I used the LCD driver of STM32L152 (the discovery board) and reached a mean current draw of 6µA. This solution has less software, which means less current, and less bugs ! Certainly the fastest way to build whatever you are building.2015-08-04 3:58 AM
Oh ! Thank you ! , didnt know that st had a stm32 with integrated lcd controller.