2018-08-19 6:46 AM
** HAL_I2C_Mem_Write_DMA not work.. **
trying to drive OLED SSD1306 0,96 inch (I2C) from STM32L031F6P6
using HAL_I2C_Mem_Write (NO DMA), worked OK
>> HAL_I2C_Mem_Write( &hi2c1, SSD1306_I2C_ADDR, 0x40, 1, &SSD1306_Buffer[SSD1306_WIDTH * i], SSD1306_WIDTH, 100);
already set DMA in Cube : I2C1_TX Dma1Channel2 MemoryToPeripheral Priority=Low
tried to set RX too (I2C1_RX Dma1Channel3 PeripheralToMemory Priority=Low) with no luck too
already try to add 4K7 Pull Up resistor on SCL and SDA
>> i2cstate = HAL_I2C_Mem_Write_DMA(&hi2c1, SSD1306_I2C_ADDR, 0x40, 1, &SSD1306_Buffer[SSD1306_WIDTH * i], SSD1306_WIDTH);
>> while(HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY);
( i2cstate always set to HAL_I2C_STATE_RESET )
anyone ? thanks...
2018-08-19 7:21 AM
Make sure the DMA clock is enabled, and that the rx/tx DMA are correctly linked to the peripheral, along with IRQ Handlers, and calls into HAL
STM32Cube_FW_L0_V1.10.0\Projects\STM32L031K6-Nucleo\Examples\I2C\I2C_TwoBoards_ComDMA\Src\stm32l0xx_hal_msp.c