cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L011F3 ADC Calibration

jason239955_st
Associate III

Hi Sir,

In STM32L0 ADC, there is a feature call ADC calibration.

I would like to know, after performing ADC calibration, do I have to do factoring using the CALFACT (calibration factor obtained after running ADC calibration) in the result I obtained from my subsequent ADC read?

OR, after the calibration, will the system perform an auto factoring and provide the corrected result in my subsequent ADC read?

Regard's

Jason

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

It's used internally by the ADC. You do not need to adjust the ADC result you get based on CALFACT.

If you feel a post has answered your question, please click "Accept as Solution".