cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L0: wrong address of COMP registers in svd file

Andreas Barth
Associate
Posted on July 02, 2018 at 13:33

Hello! I use MDK from Keil and noticed, that the address of the COMPn_CSR registers in the SystemViewer have wrong addresses.

I checked the SVD files in the latest STM32L0xx_DFP V2.0.0. The problem is the base address of the COMP peripheral. That is already the 'offset' of the first COMP1_CSR, which also has its own offset:

    <peripheral>

      <name>COMP</name>

      ...

      <baseAddress>0x40010018</baseAddress>

      ...

      <registers>

        <register>

          <name>COMP1_CSR</name>

          ...

          <addressOffset>0x18</addressOffset>

As far as I know, this SVD files are based on data provided by ST or directly provided to Keil by ST. So, I would like to asked, are there already newer files with corrected COMP peripheral addresses available or can you fix this in future files?

Thank you!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Khouloud GARSI
ST Employee

Posted on July 02, 2018 at 17:59

Hello 

andreasb.

‌,

I will check this point and update you ASAP.

Many thanks for your feedback.

Khouloud.