cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755 PSU Config Modes 2 & 3

bramble
Associate III

Hi, there's something confusing in the schematic for the H755 Nucleo's reference PCB schematic (MB1363).

I don't mind adding that I'm getting a bit tired of confusing and contradictory documentation from ST Micro.

The description of changes when configuring PSU config modes 2 and 3 are as below:

bramble_0-1747341074706.png

In the highlighted note at lower left it says that to enable Config 3: "Connect VDD_SMPS_IND_OUT to VDD_LDO".

However, looking just above at Config 2 it seems clear that VDD_SMPS_IND_OUT is already connected to VDD_LDO via the node 1V2_MCU which is always connected to both VDD_LDO and VDD_SMPS_IND_OUT.

Can somebody from please confirm how this should work?

My understanding is that the two modes can be summarised as follows (ignoring some capacitor changes):

Mode 2

  • VDD_LDO == VDD_SMPS_IND_OUT
  • VDBSD == VCAP

Mode 3

  • VDD_LDO == VDD_SMPS_IND_OUT
  • VFBSD == VDD_LDO

I need a quick answer please because I've a PCB layout needing to go to manufacture.

Thanks

0 REPLIES 0