cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755 dual core debugging issue is related to BOOT_CM4 option byte

MJack.1
Associate III

Hi all,

I'm editing this post because the forum doesn't allow me to delete it, and it might help someone else..

I was having an issue where simply generating a default NUCLEO-H755ZI-Q project from the current latest CubeMX for Cube IDE and following the debugging instructions in the following application note exactly, did not work.

I tried lots of suggestions on various posts, but for me it turned out to be that the M4 BOOT option byte was disabled, which is why I couldn't debug the M4.

I resolved it with the STLink utility.

Cheers

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Thank you @Community member​  for updating your post to share the solution.

This will help other community members finding answers to their issues ;)

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen