cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750IBT6 USB NOT DETECT IN CUSTOM BOARD

naveen
Associate III

Hi

we created custom PCB using stm32h750IBT6 MCU. in this we have added USB interface using DM & DP pins.

issue: USB interrupt in not happening when i connect USB to the connector. i have added SCHEM for reference.

considered steps in MX:

1. enabled USB_FS as HOST_ONLY,

2. given clock as 48hz from RC48,

3.  enable USB_HOST as mass storage class.

I am not understanding where I went wrong.

Screenshot 2025-04-10 183157.png



NOTE:

1.all pins are matched as per schematic.

2. in schematic i can sense 5v at out pin in ic4 as well
3. also i have removed D1 ic as well even though result



 

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @naveen 

Why Vbus sensing pin is connected to PA7? It should be configured either to PC13 or PA9 as per datasheet.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @naveen 

Why Vbus sensing pin is connected to PA7? It should be configured either to PC13 or PA9 as per datasheet.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.