HSEM causes weird jitter
- 3 replies
- 478 views
Hello,
Has anybody experienced weird jittery like behaviour when using the HSEM between two cores on the STM32H755 or another dual core MCU? This is the logic right now:
The CM4 has a 1 kHz loop that toggles a GPIO on each successful reception of data on an communication bus. On each cycle (reception of data), the CM4 writes to shared memory at address 0x38000000 which is a shared memory region located in SRAM4. Afterward the CM4 reads data at address 0x38000400 which is also in SRAM4. On every read and write, the HSEM is taken and released accordingly.
The CM7 has a 160 kHz loop that toggles a GPIO, reads from address 0x38000000, then writes to address 0x38000400. Similarly, on the CM7 each read and write operation on shared memory uses HSEM to take and release the hardware semaphore accordingly.
The problem is that with this approach, I see data at 0x38000400 update non periodically. Sometimes I see valid data after 450 us up to 7 ms. It is quite random. Is there something I'm missing?
See attached ioc file as well as code snippets for both the CM4 and CM7 side
//CM4
void cm4_task(uint16_t *pDataCmd, uint16_t *pDataFbk) {
/* Send commands */
if (HAL_HSEM_FastTake(0) == HAL_OK) {
memcpy((void*)0x38000000, pDataCmd, size);
HAL_HSEM_Release(0, 0);
}
/* Receive feedbacks */
if (HAL_HSEM_FastTake(1) == HAL_OK) {
memcpy(pDataFbk, (void*)0x38000400, size);
HAL_HSEM_Release(1, 0);
}
HAL_GPIO_TogglePin(Some_GPIO_Port, Some_Pin);
}
//CM7
extern struct command_t commands = {0};
extern struct feedback_t feedback = {0};
void cm7_task(void) {
if (HAL_HSEM_FastTake(0) == HAL_OK) {
memcpy(&commands, (void*)0x38000000, size);
// commands processed in another context
HAL_HSEM_Release(0, 0);
}
if (HAL_HSEM_FastTake(1) == HAL_OK) {
memcpy((void*)0x38000400, &feedback, size);
HAL_HSEM_Release(1, 0);
}
HAL_GPIO_TogglePin(Another_GPIO_Port, Another_Pin);
}