cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-DISCO USART issue

wjian.2
Associate III

When i want to init uart8

static void MX_USART8_UART_Init1(void)
{
huart8.Instance = UART8;
huart8.Init.BaudRate = 115200;
huart8.Init.WordLength = UART_WORDLENGTH_8B;
huart8.Init.StopBits = UART_STOPBITS_1;
huart8.Init.Parity = UART_PARITY_NONE;
huart8.Init.Mode = UART_MODE_TX_RX;
huart8.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart8.Init.OverSampling = UART_OVERSAMPLING_16;
huart8.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart8.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart8.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

/*this parte get blocked why this parte "HAL_UART_Init(&huart8) != HAL_OK"  was bad?

if (HAL_UART_Init(&huart8) != HAL_OK)
{
Error_Handler();
}

}

This should be a RCC wrong?

i have add main.c y app.c in the exhibit

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0