Skip to main content
Kranthi
Associate
January 25, 2020
Question

STM32H747 ADC Internal Reference usage and stability

  • January 25, 2020
  • 3 replies
  • 2056 views

Hello

I am new to STM32 family and currently I was working on STM32H747I-DISCO board with HAL device support.

Is it possible to change the ADC reference from external Vref+ to internal Vref ? if possible how to configure? why because there is no parameter to configure ADC reference in HAL libraries.

And while using with external reference voltage Vref+ the ADC count was fluctuating even if the configured ADC channel was connected to ground. How to stabilize it?

Thank You

This topic has been closed for replies.

3 replies

berendi
Principal
January 25, 2020

If there is a way, then you can find it in the reference manual.

HAL can't do everything that the MCU can do. The reference manual is the authorative documentation, HAL is a collection of examples that helps beginners getting started.

Kranthi
KranthiAuthor
Associate
January 25, 2020

Thank you for your quick response.

I found VREFBUF registers in reference manual. Is it possible to configure VREFBUF registers while configuring ADC ?

In my board Vref+ was connected to +3.3.V supply, is it possible to configure internal reference?

berendi
Principal
January 26, 2020

Change VREF before configuring the ADC, because the ADC should be recalibrated afterwards anyway. But don't expect much improvement.

Getting stable ADC readings requres noise-free Vdda, Vssa and Vref supplies, something that cannot be fixed in software.

Kranthi
KranthiAuthor
Associate
January 27, 2020

Thank you

oleksandr.karbivsky
Senior II
January 27, 2020

>> Is it possible to change the ADC reference from external Vref+ to internal Vref ?

No. The internal voltage reference is internally connected to the input channel ADC3 VINP[19]. The internal voltage reference can be monitored to have a reference point for evaluating the ADC VREF+ voltage level.

From reference manual "26.4.35 Monitoring the internal voltage reference".

Kranthi
KranthiAuthor
Associate
January 28, 2020

But according to chapter 28 Voltage Reference Buffer you can configure Internal reference voltage for ADC and DAC reference voltage and you can also select the voltage levels with VREFBUF_CSR.

I tried and configured for 1.5V, it is working.