cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745/747 power supply configuration for VOS0?

In DS12923 (Rev 1), it is stated that VOS0 is only available with LDO, but it is not clear if LDO-Only mode is required or SMPS-LDO cascaded mode is okay.

First,

3.5.3 Voltage regulator (SMPS step-down converter and LDO) says

• Run mode (VOS0 to VOS3)

– Scale 0: boosted performance (available only with LDO regulator)

And

Table 24. Supply voltage and maximum frequency configuration

Note 1 says

VOS0 (power scale 0) is not available when the SMPS step-down converter directly supplies VCORE.

which suggests SMPS-LDO cascaded mode can be used.

However,

3.5.4 SMPS step-down converter says

1. When the SDEXTHP bit is equal to 1 in PWR_CR3, the SMPS step-down converter is forced to High-performance mode ...

which suggest that SMPS is not suit for boosted performance (480MHz with VOS0) at all (all it can do is to supply up to high-performance mode --- 400MHz with VOS1).

Thoughts?

Btw, Nucleo-H745ZI-Q is configured for Direct-SMPS mode, so it seems that 480MHz applications/examples (if any) are out of spec without mangling with the power supply configuration.

@TDK​ May be related with

https://community.st.com/s/question/0D50X0000BVpWdpSQF

A note. The Nucleo-H745ZI-Q with default direct-SMPS can be run time configured and execute at 480MHz with VOS0 when CM4 is not clocked (BOOT_CM4 turned off), so the configuration is not checked software-wise, and can be set hardware-wise.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0