cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743VIT6. FMC for SDRAM

OIrin.1
Associate II

Hi,

Is SDRAM over FMC supported in STM32H743VIT6 MCUs? I can't see this option in CubeMX, only NOR Flash/PSRAM/SRAM/ROM/LCD and NAND Flash. The datasheet says that SDRAM is not supported in LQFP144 packages, but my one is LQFP100.

Looking forward for any help.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

Even fewer pins, so assuming more of the pins you'd need are absent...

Try the Data Sheet and then play Pin Bingo

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

FMC_SDNRAS, FMC_SDNCAS ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

SDRAM is not available on the LQFP100 either. FMC_A0, among many others, is absent on the pinout.

If you feel a post has answered your question, please click "Accept as Solution".
OIrin.1
Associate II

Thank you very much Tesla and TDK. I have checked the pinout once more and now I see that some necessary pins for SDRAM support are absent in LQFP100 package. It's a pity.