cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735IGT MCU- ADC DMA Multi Channel Data is Not Obtained

SSAIL2023
Associate II

In STM32H735IGT mcu I have initialized ADC1 and ADC3 in DMA method, also FreeRTOS is initialized. But ADC1 adc data is not obtained. But i can read ADC3 data. What may be the issue? One of the differences i have identified is continouous DMA request enable option is not available in ADC1. Also I have tried with basic adc polling method still ADC1 is not working. System clock I have enabled as timer 6 since for FreeRTOS req system clock should not be systick. Attached below  code.

0 REPLIES 0