STM32H7 series resistors in data lines ?
With a 400MHz clock and very high speed ports, I was assuming the faster data lines would need series resistors to avoid reflections in the way things like FPGAs do. But I've just noticed the evaluation board doesn't have any and routes even high speed lines off the board and to the LCD without any. The DSA lines are even labelled at 500MHz clocking.
Do STM MCUs have some way to avoid signal reflection (internal resistors ?) or should I leave them in anyway. It would save quite a bit of board space to remove them as I've got quite a lot of buses going between multiple MCUs.