cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 支持的协议

hanqingze
Associate III

STM32H7 can support SPI communication, Parallel communication, GPIO analog SPI communication, but can it support TTL, SDR CMOS, JESD204B protocol communication? Or what should I do if I want STM32 to implement these protocols?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mƎALLEm
ST Employee

Hello,

STM32 does not implement JESD204B standard. GPIO emulation is the only solution available which is not an easy task taking into account timing constraints etc ..

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

>>Or what should I do if I want STM32 to implement these protocols?

Bolt on an FPGA / CPLD ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..