2025-01-17 1:26 PM - edited 2025-01-17 1:27 PM
So I've got a program with a fast tight loop doing some minimal things, and the rest is housekeeping/UI stuff in the main loop. When I enabled ICACHE, the speed of the tight loop increased DRAMATICALLY and overall the process is faster at basically everything. A colleague of mine said that he uses the DCACHE also and that for his application on an H7, the DCACHE made a huge performance improvement. But, as far as I can measure (which is toggling GPIO pins at critical sections of code and measuring the time with o-scope), the DCACHE made no difference on or off.
So for now I 'm just leaving it off because I know I need to be careful with DCACHE and my SD Card etc. and it's easier to just leave it off, but I'm wondering what areas/use cases is the DCACHE actually supposed to improve with this chip?
2025-01-17 1:51 PM
Per the Reference Manual the connectivity for the DCACHE (4KB) is the OCTOSPI and FMC, so code/data on external memories likely to be where you'd see it.
The SRAMs all look to be relatively closely coupled
2025-01-17 3:25 PM
Thanks, that's a good point. I'm not using the OCTOSPI or the FMC for anything, so that would correlate to what I'm seeing.
2025-01-17 3:34 PM
Not sure the caching would impact the SDMMC in this context.
The H7 is a particularly odd beast, designed as a dual core, with dual ported memories. The F7 on the other hand can use the DTCM for SDMMC DMA, and that's not cached.
You want the DMA 4-byte aligned. On the H7 the cache lines are 32-byte aligned, and SDMMC there is workable with care, as the clear/invalidate by address need to span the buffer, it they are miss-aligned you can get collateral damage to structures directly abutting the SDMMC DMA buffer.