2026-03-25 2:04 AM - last edited on 2026-03-25 2:07 AM by mƎALLEm
Hello,
Is my understanding correct that it's impossible to internally detect short (<100ns) drops of VCORE internally?
Reading RM0481 page 154 it seems impossible to directly monitor VCORE through the tamper mechanism which I assume forces the use of an ADC+WDG, which probably puts the detection range in the µs? Which means the target is sensitive to fault injections?
2026-04-09 7:53 AM
Hello @gquere and welcome to the community;
As mentioned in the datasheet the minimum TS_VCore is 1 µs, with ADC sampling time when reading the VCORE voltage. Note that the VCORE monitoring characteristics value is specified by design and not tested in production.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.