cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with USB Power Delivery Sink on STM32 - ERROR with Trace_Notif :78

vladovlado
Associate II

Hi everyone,

I’ve been following the official ST guide for setting up USB Power Delivery (PD) Sink on an STM32 device, as outlined here: Getting started with USB-Power Delivery Sink.

I successfully compiled and flashed the firmware onto my NUCLEO-G071RB board. When I tried connecting my setup (NUCLEO-G071RB + X-NUCLEO-SNK1M1) to an external monitor via USB-C to test the power delivery negotiation, I encountered an issue: `ERROR with Trace_Notif :78`.

The issue can be caught when debugging using STM32CubeMonitor-UCPD.
I've attached the whole trace.

Kind regards,
Vlado

3 REPLIES 3
FBL
ST Employee

Hi @vladovlado 

Would you attach your test case to reproduce the issue on my end?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

Hi @FBL 

Here is the zip of the whole project + traces with another source device.
The ERROR happens when I plug the cable from laptop/monitor to snk1m1.

Update on the project:
The PD part works, but the source of the ERROR trace is still unknown. The error message is some kind of a timeout but the question remains, why does it trigger?

Also, I would kindly ask you to review https://community.st.com/t5/stm32-mcus-embedded-software/vdm-issue-pe-send-notsupported-on-stm32g071rb-snk1m1-sink-mode/td-p/786718
since it's the same hardware.

Kind regards,
Vlado

I am also getting this error using an STM32G0B1 with a TCPP03-M20.

NMartin_1-1744756930601.png