cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G030F6 USART1 received interrupt not working

dsapk.1
Associate

Hi I am using ​STM32G030F6 I am try to programing UART 1&2. UART2 is working fine with transmit & receive data. But UART1 only able to transmit data not able received.

Please let me is there any settings is required.​

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KDJEM.1
ST Employee

Hi @dsapk.1​ and welcome to the Community :),

Try to use only USART1 and check if you can receive data.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.