cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0 Lsecss issue

oziesin
Associate III

Hi all,

I enabled LSECSSON register after select rtc clock as said from RM.

I did not have any problem but if i shutdown power and power on , device used LSI as a rtc source and it cannot start LSE. Why this is happening ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @oziesin​ ,

Which pin of the chip are you using to start from shutdown mode ?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
oziesin
Associate III

Manually, I plug off of energy pin and plug in again.

Hi @oziesin​ ,

Make sure you are well powering OFF the device.

As you know at power ON, device start from default configuration (all status/config bits at their default status), and so behaviour at each power-on should be always the same. 

When you switch poweron -> poweroff, I would suggest to check that VDD goes to ‘0’ and stay enough time w/o power.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen