cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F777 HAL SDMMC

SHans.1
Associate

Hi.

Im experiencing a race condition in SDMMC_CmdReadSingleBlock. (being called trough HAL_SD_ReadBlocks_DMA).

SDMMC_CmdReadSingleBlock calls SDMMC_SendCommand in order to start transfer.

Then it calls SDMMC_GetCmdResp1 to verify that transfer is started.

Problem occurs when code is interrupted (by unrelated interrupts) between SDMMC_SendCommand and SDMMC_GetCmdResp1.

If the interruption last long enough, transfer will be finished and HAL_SD_IRQHandler will be executed before SDMMC_GetCmdResp1 is allowed to run.

HAL_SD_IRQHandler clears the SDMMC-flag that SDMMC_GetCmdResp1 is looking for, and SDMMC_GetCmdResp1 eventually returns with timeout-error.

This in turn causes HAL_SD_ReadBlocks_DMA to return with error.

I am able to disregard the error returned by HAL_SD_ReadBlock_DMA by verifying through HAL_SD_RxCpltCallback that transfer actually were successful.

Problem is that SDMMC_GetCmdResp1 has such a long timeout condition.

The timeout is hardcoded to 5s with a macro. Does it really need to be this long?

All it does is to wait for a command-respons. It should be a matter of ms, right?

But actually it gets even worse.

The timeout is implemented as a while-loop with a counter.

It does not take into consideration that it can be interrupted!

In my case, SDMMC_GetCmdResp1 times out after 15s.

So im wondering, will there be any changes to this driver in the near future?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0