STM32F769I-Discovery - upload to QSPI Flash from uSD card, and display on LCD
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-04-29 6:37 AM
Posted on April 29, 2017 at 15:37
To prove a bad thing can get worse, I stitched together some of the HAL example code
This project takes RGB8888 bitmaps [max of 25] and uploads them to the QSPI Flash on-board. It outputs information on uart 1
https://github.com/ProjectsByJRP/uSDcard_to_QSPI_flash
This project takes the bitmaps in the QSPI flash and displays them on the on-board LCD. output on uart1
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0