cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32F746g-disco LTDC-FMC

Hosting
Associate III
Posted on June 02, 2018 at 23:49

Hello! I'm trying to run an LCD installed on the board Stm32F746g-disco, memory and the display are successfully initialized, but I can not fill the display with color. What is wrong in my project? Maybe someone has a working draft for an example?

10 REPLIES 10
Posted on June 04, 2018 at 15:09

What a shame. I've never had much luck with it. If would be a great asset if it worked - it seems to be 99% of the way there but never quite produce something usable for me.