2016-02-15 6:52 AM
Hi All,
I would like to know if there is any demo code to connect the discoverySTM32F4DIS-CAM
module camera to the STM32F746G-DISCO camera interface and display the camera image on the LCD. I have not found any code that demonstrates this so far. Can anyone help with this. Thanks in advance. #stm32f746g-disco #stm32f7 #camera2016-12-08 6:01 AM
Hi
to_deletefirmware
,I recommend that you refer to both DCMI examples in
' DCMI_CaptureMode' and 'DCMI_SnapshotMode' avaialble for STM32756G -EVAL and STM32F769I -EVAL at following path respectively:-Walid F-
if the response is helpful , click on correct button