2016-12-16 2:08 AM
Hello,
I have problems with a STM32F746 and DCache. Without DCache my software runs perfectly. If I enable the DCache (first invalidate it and the Enable), then I can't start the board.
I have check my source code, the document (Programmer Manual from STM32, the AN4839 [L1-Cache on STM32F7], the errata of Cortex M7 and STM32F746, but I have no idea.
After a power on, the processor runs in a hard fault. The IMPRECISERR in System Control - Bus Fault Status register and the AXIM-Bit in ABFSR (Auxiliary Bus Fault Status register) are set. The AXIM Type is 2.
If I understand this bits right then someone write (due to the IMPRECISERR) on wrong address via the AXIM-Bus. The AXIM-Slaves are the FLASH, SRAM, FMC and QUAD-SPI. I don't use FMC and Quad-SPI. FLASH is read only - therefor I suggest the problem is according to the SRAM. This can match to a problem with the DCache. (Incorrect invalidate?)
In the AN4667 (STM32F7 Series system architecture and performance) I found one sentence which I don't understand: Page 43 - last sentence (Chapter 4.2 Tips, last sentence).
'It is not recommended to enable the cache before calling the main function, that is, before the scatter load phase, because a hard fault may occur'.
What means this? Why a hard fault does occur? Is this a reason for my problem?
Best regards, Michael
#ada #stm32f7 #startup #dcache2016-12-21 5:28 AM
Hello,
thanks a lot for helping. I found my mistake. The problem was in the Invalidate procedure of the cache. I had unroll the two loops (for ways and sets). If I use exactly the same routine like in core_cm7 then my ada project works fine.
sets = (uint32_t)(CCSIDR_SETS(ccsidr));
do {
ways = (uint32_t)(CCSIDR_WAYS(ccsidr));
do {
SCB->DCISW = (((sets << SCB_DCISW_SET_Pos) & SCB_DCISW_SET_Msk) |
((ways << SCB_DCISW_WAY_Pos) & SCB_DCISW_WAY_Msk) );
#if defined ( __CC_ARM )
__schedule_barrier();
#endif
} while (ways--);
} while(sets--);
__DSB();�?�?�?�?�?�?�?�?�?�?�?�?
The problem wasdefinitely my bad Invalidation of the Cache.
Only one think I don't understand: is there a timing issue or what could be the problem?
Best regards Michael
2018-02-06 1:28 AM
I know, there is later answer, but I had similar problem now.
I think, the cause of this issue is overwriting of local variables on the stack on background by L1 cache, while the loop is in progress. The same problem was in SCB_DisableDCache() function. This problem was already solved.
Update of core_cm7.h file from latest version of CMSIS (I think it is V5.2.0 now) is need.
The variables sets, ways, cssidr are declared with register keywords -> then they are not located in RAM and cache background processes has not impact on them.
Unfortunately only SCB_DisableDCache() was fixed in CMSIS V5.2.0.
But, after adding the register keyword to variables in SCB_InvalidateDCache() function, it helps me.
for example:
register uint32_t ccsidr;
register uint32_t sets; register uint32_t ways; SCB->CSSELR = 0U; /*(0U << 1U) | 0U;*/ /* Level 1 data cache */ __DSB(); ccsidr = SCB->CCSIDR; /* invalidate D-Cache */ sets = (uint32_t)(CCSIDR_SETS(ccsidr)); do { ways = (uint32_t)(CCSIDR_WAYS(ccsidr));do {
SCB->DCISW = (((sets << SCB_DCISW_SET_Pos) & SCB_DCISW_SET_Msk) | ((ways << SCB_DCISW_WAY_Pos) & SCB_DCISW_WAY_Msk) ); &sharpif defined ( __CC_ARM ) __schedule_barrier(); &sharpendif } while (ways-- != 0U); } while(sets-- != 0U);