cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f746 discovery external memory memory mapped

Hi, In STM32746 discovery, We are using external flash memory in memory-mapped. My doubt is that all external flash memory supports memory-mapped mode or few specific? Can I use MX35LF1GE4AB in memory map mode?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

It's not the memory chip that is supporting this mode, it's the microcontroller translating things for you. Any chip which is supported by the FMC will be able to be memory mapped.

If you feel a post has answered your question, please click "Accept as Solution".

@TDK​ Thanks for the reply. With QSPI flash also we can do memory-mapped (not sure about spi).

TDK
Super User

QUADSPI memory can also be memory mapped.

SPI memory cannot, unless there's a compatible QUADSPI mode for them, which might be the case, not sure.

If you feel a post has answered your question, please click "Accept as Solution".