Skip to main content
Associate
July 13, 2024
Solved

stm32f722 SWD MEM-AP ports

  • July 13, 2024
  • 2 replies
  • 2003 views

I'm trying to see what's possible in terms of a bootloader in a custom application of an stm32f722.

 

We have an external 2-megabyte flash chip on the QSPI bus, along with the internal 512-kilobyte flash.  I'd like to make the bootloader stored on internal flash as tiny as possible; the best way to do this is to make it evaluate the image stored on internal flash as well as external, and simply jump to whichever one passes this evaluation.  I'd then put the code to handle USB DFU mode, SPI download mode, UART download mode, etc., all on the external flash, and run it from there only if needed.

 

This requires being able to write that code into the external flash using SWD (further upgrades can be done over any of the protocols above, but for the first time we need to use SWD as the code isn't on the device yet to do the other protocols).  What I can't tell is whether the SWD implementation on this chip allows writes to flash chips mapped on the external QSPI bus -- does the MEM-AP port (which I assume exists, because it's possible to update the internal flash over SWD) cover the registers used to configure QSPI?  Does it cover the 0x80000000 - 0x9fffffff memory range that maps to the QSPI bus?

 

Is the set of SWD ports that the stm32f722 has, documented anywhere?  I could not find it in either the datasheet or the reference manual (RM0431).  I've read the "ARM Debug Interface v5 Architecture Specification" doc from ARM, but that only explains how the protocol works and what the ports need to look like, not how they're implemented.  I also don't see any app notes about this -- the closest one is AN4989, the "debug toolbox", but it doesn't seem to cover the available ports, only how to mess with the core's execution.

 

Thanks for any information!

This topic has been closed for replies.
Best answer by STOne-32

Dear @bkadzban ,

To first program the QSPI flash , you need to use SWD to connect to the MCU STM32F7 and write a small bootstrap code inside the Internal RAM that will activate the QSPI interface controller - setup the right configuration of the external memory and then Write the the first code thru the CPU/ RAM buffer to it . You can not program directly the QSPI memory thru SWD without MCU setup.

Hope it helps you ,

STOne-32

2 replies

STOne-32
STOne-32Best answer
ST Technical Moderator
July 13, 2024

Dear @bkadzban ,

To first program the QSPI flash , you need to use SWD to connect to the MCU STM32F7 and write a small bootstrap code inside the Internal RAM that will activate the QSPI interface controller - setup the right configuration of the external memory and then Write the the first code thru the CPU/ RAM buffer to it . You can not program directly the QSPI memory thru SWD without MCU setup.

Hope it helps you ,

STOne-32

bkadzbanAuthor
Associate
July 13, 2024

Thank you!

 

That made me think this functionality might already exist in a higher level tool, and for initial programming, using such a higher level tool might be fine.  (It won't require permanent support on the device.)  I planned to use OpenOCD to program the internal-flash bootloader before asking this question, and it turns out [1] that OpenOCD does already have a driver for the STM QSPI bus.

 

[1] https://openocd.org/doc/html/Flash-Commands.html#index-stmqspi-1

 

I'm not 100% sure the particular serial flash chip I plan to use is known to the OpenOCD code, but it can definitely send arbitrary commands, so it can be made to work.

 

So I think this will be fine for my needs.  Thanks again!