cancel
Showing results for 
Search instead for 
Did you mean: 

Please tell me how to calculate the dead time or determine dead time in this figure. 

Ken Inoue
Associate III
Posted on April 16, 2017 at 17:39

Thank you for your patronage.  Please tell me how to calculate the dead time or determine dead time in this figure. 

I understand that

HCLK = 84MHz

Prescaler = 83

Counter Period = 99

Pulse = 20

Dead Time = 150

so frequency = 10kHz, Duty ratio = 20%. 

But I can't understand dead time is 2?s.

#dead-time
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Haris Riaz
Associate
Posted on April 19, 2017 at 00:20

Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.

So for 2us, deadtime value should be like 168. 

Thats what i think.

View solution in original post

5 REPLIES 5
Posted on April 17, 2017 at 02:16

No dead time is defined

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 17, 2017 at 10:58

I'm sorry. Dead time =150.

Haris Riaz
Associate
Posted on April 19, 2017 at 00:20

Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.

So for 2us, deadtime value should be like 168. 

Thats what i think.

Posted on April 19, 2017 at 00:21

this assumes Tdts = internal clock..

Posted on April 20, 2017 at 11:24

Thank you very much.