Skip to main content
clement
Associate
July 4, 2013
Question

STM32F4xx CAN2 problem

  • July 4, 2013
  • 2 replies
  • 957 views
Posted on July 04, 2013 at 15:18

Hi,

I work with an STM32F405 and i cannot use the CAN2. 

Now, I do some tests on the discovery board on an STM32F407. And with the same code developed for CAN2 used with CAN1 all seems good. 

I think, that I have forgotten something, but what?

This is my can configuration :

static void CAN_Configuration( void )

{

  

  RCC_APB1PeriphClockCmd( RCC_APB1Periph_CAN2, ENABLE );

  

  CAN_InitTypeDef       CAN_InitStructure;

  CAN_FilterInitTypeDef CAN_FilterInitStructure;

           

  // CAN register init 

  CAN_DeInit( CAN2 );

  CAN_StructInit( &CAN_InitStructure );

  

  // CAN cell init 

  CAN_InitStructure.CAN_TTCM      = DISABLE;

  CAN_InitStructure.CAN_ABOM     = ENABLE;

  CAN_InitStructure.CAN_AWUM    = ENABLE;

  CAN_InitStructure.CAN_NART      = DISABLE;

  CAN_InitStructure.CAN_RFLM      = DISABLE;

  CAN_InitStructure.CAN_TXFP       = DISABLE;

  CAN_InitStructure.CAN_Mode       = CAN_Mode_LoopBack; /* todo CAN_Mode_Normal */

  // CAN Baudrate = 175kbps (CAN clocked at 42 MHz) 

  CAN_InitStructure.CAN_SJW        = CAN_SJW_1tq;

  CAN_InitStructure.CAN_BS1         = CAN_BS1_6tq;

  CAN_InitStructure.CAN_BS2         = CAN_BS2_8tq;

  CAN_InitStructure.CAN_Prescaler  = 16u;

 

  CAN_Init( CAN2, &CAN_InitStructure );

  

  // Activate CAN in debug mode

  CAN_DBGFreeze( CAN2, DISABLE );

  // CAN filter init 

  CAN_FilterInitStructure.CAN_FilterNumber         = 0u;

  CAN_FilterInitStructure.CAN_FilterMode           = CAN_FilterMode_IdMask;

  CAN_FilterInitStructure.CAN_FilterScale          = CAN_FilterScale_32bit;

  CAN_FilterInitStructure.CAN_FilterIdHigh         = 0x0000u;

  CAN_FilterInitStructure.CAN_FilterIdLow          = 0x0000u;

  CAN_FilterInitStructure.CAN_FilterMaskIdHigh     = 0x0000u;

  CAN_FilterInitStructure.CAN_FilterMaskIdLow      = 0x0000u;  

  CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0u;

  CAN_FilterInitStructure.CAN_FilterActivation     = ENABLE;

  CAN_FilterInit( &CAN_FilterInitStructure );

}

#can #problem #stm32f4
This topic has been closed for replies.

2 replies

clement
clementAuthor
Associate
July 4, 2013
Posted on July 04, 2013 at 15:41

Problem solved : 

  RCC_APB1PeriphClockCmd( RCC_APB1Periph_CAN2, ENABLE ); -->   RCC_APB1PeriphClockCmd(( RCC_APB1Periph_CAN1 | RCC_APB1Periph_CAN2 ), ENABLE );

 CAN_FilterInitStructure.CAN_FilterNumber         = 0u;                           --> CAN_FilterInitStructure.CAN_FilterNumber         = 14u; 

Tesla DeLorean
Guru
July 4, 2013
Posted on July 04, 2013 at 16:12

The filter are certainly one of the issues, though I seem to recall you can change the split between the controllers.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..