cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery interrupt on PortD Pin0

bjoernprecht
Associate
Posted on March 30, 2013 at 15:09

Hello,

i used a STM32F4Discovery. My code is at the end of this text. The programm should release a interrupt by rising edge on PortD Pin0. Then the LED toggle on PortD Pin14. This does not work. Where is the mistake?

Thank you.

int main (void) {

  SystemInit();

  GPIO_InitTypeDef GPIO_InitStructure;

  EXTI_InitTypeDef EXTI_InitStructure;

  NVIC_InitTypeDef NVIC_InitStructure;

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOD, &GPIO_InitStructure);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOD, &GPIO_InitStructure);

  SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOD, EXTI_PinSource0);

  EXTI_InitStructure.EXTI_Line = EXTI_Line0;

  EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

  EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;

  EXTI_InitStructure.EXTI_LineCmd = ENABLE;

  EXTI_Init(&EXTI_InitStructure);

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);

  NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;

  NVIC_Init(&NVIC_InitStructure);

    while(1)   {

        }

}

void EXTI0_IRQHandler(void){

  if(GPIO_ReadOutputDataBit(GPIOD, GPIO_Pin_14)){

    GPIO_WriteBit(GPIOD, GPIO_Pin_14, RESET);

  }else{

    GPIO_WriteBit(GPIOD, GPIO_Pin_14, SET);

  }

    EXTI_ClearITPendingBit(EXTI_Line0);

}
2 REPLIES 2
Posted on March 30, 2013 at 16:00

In the CMSIS model SystemInit() is called prior to main(), not a good plan to call it again.

EXTI is on the SYSCFG unit, you must enable it's clock.

  /* Enable SYSCFG clock */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

Also you should check/clear the interrupt source on entry, so as not to cause the handler to re-enter via a tail-chaining hazard.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bjoernprecht
Associate
Posted on April 01, 2013 at 13:48

Thank you