cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446

Posted on December 15, 2014 at 09:11

Thanks to Mayla for updating us. Again, it's a pity the announcement is locked and we can't discuss the merits of the new STM32 family members...

Some remarks to the text in the announcement:

- SPDIF is Rx only, if I understood right

- the 7 I2S channels are to be read as 3 simplex I2S shared with 3 SPI, plus 2 duplex I2S

- QUAD-SPI (YES way to go, ST!) - it's not ''dual'' as ''two pieces'', but as ''dual mode'' - can work ''normally'' through registers, but also through memory mapped acces (way to go, again!)

- LCD support - it's just a marketing fluff, if I understood correctly, it means ''you can attach a display with controller supporting 8080/6800-style interface, through FMC''

- 180MHz system clock

- the strange combination of peripherals hints a strong customer with particular requirements ... ;)

Btw. anybody noticed this is the first even-numbered STM32F4? :)

JW

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0