2014-12-16 5:15 AM
My company has developed a board with a STM32F207IG and RMII ethernet which is working fine. Now they have given me the same board with a STM32F439II fitted, and here I can not get the ethernet to work. The CPUs should be pin compatible. After enabling the receive all packets and forward error frames flags, I can see the DMA writing in the receive buffer, but the data is not good. I have tried to use the same clock settings as the first board, but the error remained.
Fyi : IDE : Raisonce Ride 7 v7.48.13.0324, Rkit-ARM v1.52.13.0324LwIP v1.4.1Standard Peripheral Library : STM32F4xx_StdPeriph_Driver_v1.4.0 (project dates from before Cube) ETH_StructInit(Ð_InitStructure); /* Fill ETH_InitStructure parametrs */ /*------------------------ MAC -----------------------------------*/ ETH_InitStructure.ETH_AutoNegotiation = ETH_AutoNegotiation_Enable; ETH_InitStructure.ETH_LoopbackMode = ETH_LoopbackMode_Disable; ETH_InitStructure.ETH_RetryTransmission = ETH_RetryTransmission_Disable; ETH_InitStructure.ETH_AutomaticPadCRCStrip = ETH_AutomaticPadCRCStrip_Disable; ETH_InitStructure.ETH_ReceiveAll = ETH_ReceiveAll_Enable; ETH_InitStructure.ETH_BroadcastFramesReception = ETH_BroadcastFramesReception_Enable; ETH_InitStructure.ETH_PromiscuousMode = ETH_PromiscuousMode_Disable; ETH_InitStructure.ETH_MulticastFramesFilter = ETH_MulticastFramesFilter_Perfect; ETH_InitStructure.ETH_UnicastFramesFilter = ETH_UnicastFramesFilter_Perfect;#ifdef CHECKSUM_BY_HARDWARE ETH_InitStructure.ETH_ChecksumOffload = ETH_ChecksumOffload_Enable;#endif /*------------------------ DMA -----------------------------------*/ /* When we use the Checksum offload feature, we need to enable the Store and Forward mode: the store and forward guarantee that a whole frame is stored in the FIFO, so the MAC can insert/verify the checksum, if the checksum is OK the DMA can handle the frame otherwise the frame is dropped */ ETH_InitStructure.ETH_DropTCPIPChecksumErrorFrame = ETH_DropTCPIPChecksumErrorFrame_Enable; ETH_InitStructure.ETH_ReceiveStoreForward = ETH_ReceiveStoreForward_Enable; ETH_InitStructure.ETH_TransmitStoreForward = ETH_TransmitStoreForward_Enable; ETH_InitStructure.ETH_ForwardErrorFrames = ETH_ForwardErrorFrames_Enable; ETH_InitStructure.ETH_ForwardUndersizedGoodFrames = ETH_ForwardUndersizedGoodFrames_Enable; ETH_InitStructure.ETH_SecondFrameOperate = ETH_SecondFrameOperate_Enable; ETH_InitStructure.ETH_AddressAlignedBeats = ETH_AddressAlignedBeats_Enable; ETH_InitStructure.ETH_FixedBurst = ETH_FixedBurst_Enable; ETH_InitStructure.ETH_RxDMABurstLength = ETH_RxDMABurstLength_32Beat; ETH_InitStructure.ETH_TxDMABurstLength = ETH_TxDMABurstLength_32Beat; ETH_InitStructure.ETH_DMAArbitration = ETH_DMAArbitration_RoundRobin_RxTx_2_1; /* Configure Ethernet */ EthStatus = ETH_Init(Ð_InitStructure, DP83848_PHY_ADDRESS);I created 3 small test projects, starting from the ''tcp echo server'' demo. One project for the each board I have here. On the STM324x9I-EVAL board the program is working with ethernet in MII mode. On our 207 board the code is also working with ethernet in RMII mode. But I can't get it to work on the 439. Am I overlooking a change in the 439 ? Does anybody have any idea ?2014-12-16 1:18 PM
Are you shure they are pin compatible?
What about C6? Where is it connected to now.... 207 RFU (reserver for future use) 439 PDR-On (power-down reset)2014-12-16 10:04 PM
2014-12-17 3:25 AM