cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f429i-disc1 and breadboards?

bengt
Associate
Posted on January 15, 2016 at 22:27

I thinking of ordering a stm32f429i-disc1 discovery kit and I was wondering how I can mount this on a breadboard as is has double rows of pin on both the left and right side?  The breadboards that I know of are made for single rows of pins and would not work.

Please, explain or show me a breadboard that would work. Thanks!

#breadboard #stm32f429i-disc1 #think-differently
4 REPLIES 4
Posted on January 15, 2016 at 22:37

It's not a good board for prototyping. The LCD+SDRAM soak up a lot of the pins. You should review the User Manual, and go over the pins/resources you think you need. Think about how many pins you actually need to get over to the bread board, or use wire-wrap techniques. Better yet find an STM32 based ''break-out'' board where you can actually get to signals you can use.

The

http://www.st.com/web/catalog/tools/FM116/CL1620/SC959/SS1532/LN1848/PF262395?icmp=tt2951_gl_pron_oct2015&sc=stm32f469idiscovery

has an Arduino shield connector, and there are

https://www.google.com/search?q=arduino+breadboard+shield&biw=1496&bih=896&tbm=isch&imgil=q7oHHnVBnTdF0M%253A%253Bb_dQTO_j4iAzeM%253Bhttp%25253A%25252F%25252Fwww.dx.com%25252Fp%25252Farduino-prototype-shield-with-mini-breadboard-65273&source=iu&pf=m&fir=q7oHHnVBnTdF0M%253A%252Cb_dQTO_j4iAzeM%252C_&u...

.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ferhatyol-23
Senior
Posted on January 15, 2016 at 22:42

No, You mustn't use breadboard. You can use female to male jumper wires. 

Mark Edwards
Associate II
Posted on January 26, 2016 at 19:33

Example of Connectors - Mouser UK - PN. 855-M20-6103245

(Usually use a Samtec part but can't find the part no.)

Breadboard - Proto Advantage - PN. SBBTH4080-1

Pic - Test board to check connection between STM32F429 Disco Bd and FPGA before generating PCB.

0690X00000603M9QAI.jpg
TarekB-ST
Associate III
Posted on January 27, 2016 at 10:36

I suggest using the

http://www.st.com/st-web-ui/active/en/catalog/tools/PF262637

(Nucleo 144)