cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 TIM *** Question

Franksterb92
Senior

im confused about the TIMPRE bit in the RCC_DCKCFGR does it only effect the apb1 and not apb2 timers cause the way it describes this bit it acts like the apb2  can be times 4 because it says PPREx so 1 or 2  but on cube mx im noticing when u enable the timer prescaler the only timers effected are the apb1 timers 

0 REPLIES 0