cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429-Generating variable PWM using DMA

Hobbyist
Associate II
Posted on June 07, 2017 at 12:59

Hi,

Variable PWM is not working. So i looked at theexample code provided in 'STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_DMA'

Based on example, modified code generated using cubeMx.

Please can anyone tell me the

1) What is Repetition counter(

htim8.Init.RepetitionCounter) ? how it effects timer and PWM?

2) Where is the mistake in below code?

In main.c

int main(void)
{
 HAL_Init();
 SystemClock_Config();
 lowPass();
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM8_Init();
 while(1){
 if(htim8.State==HAL_TIM_STATE_READY){
 HAL_TIM_PWM_Start_DMA(&htim8,TIM_CHANNEL_3,(uint32_t *)&SineLookupTable[0],PWM_SZ);
 }
 }
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base){
 __HAL_RCC_TIM8_CLK_ENABLE();
 hdma_tim8_ch3.Instance = DMA2_Stream4;
 hdma_tim8_ch3.Init.Channel = DMA_CHANNEL_7;
 hdma_tim8_ch3.Init.Direction = DMA_PERIPH_TO_MEMORY;
 hdma_tim8_ch3.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim8_ch3.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim8_ch3.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_tim8_ch3.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_tim8_ch3.Init.Mode = DMA_CIRCULAR;
 hdma_tim8_ch3.Init.Priority = DMA_PRIORITY_LOW;
 hdma_tim8_ch3.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
 if (HAL_DMA_Init(&hdma_tim8_ch3) != HAL_OK) {
 _Error_Handler(__FILE__, __LINE__);
 }
 __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_CC3],hdma_tim8_ch3);
 /* TIM8 interrupt Init */
 HAL_NVIC_SetPriority(TIM8_BRK_TIM12_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM8_BRK_TIM12_IRQn);
 HAL_NVIC_SetPriority(TIM8_UP_TIM13_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM8_UP_TIM13_IRQn);
 HAL_NVIC_SetPriority(TIM8_TRG_COM_TIM14_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM8_TRG_COM_TIM14_IRQn);
 HAL_NVIC_SetPriority(TIM8_CC_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM8_CC_IRQn);
}
static void MX_TIM8_Init(void){
 TIM_ClockConfigTypeDef sClockSourceConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 TIM_OC_InitTypeDef sConfigOC;
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig;
 htim8.Instance = TIM8;
 htim8.Init.Prescaler = 100;
 htim8.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim8.Init.Period = TIM8_IR_CNT_VAL;
 htim8.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim8.Init.RepetitionCounter = PWM_SZ;
 if (HAL_TIM_Base_Init(&htim8) != HAL_OK) {
 _Error_Handler(__FILE__, __LINE__);
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim8, &sClockSourceConfig) != HAL_OK){
 _Error_Handler(__FILE__, __LINE__);
 }
 if (HAL_TIM_PWM_Init(&htim8) != HAL_OK){
 _Error_Handler(__FILE__, __LINE__);
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim8, &sMasterConfig) != HAL_OK){
 _Error_Handler(__FILE__, __LINE__);
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = TIM8_IR_DUTY_VAL;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
 if (HAL_TIM_PWM_ConfigChannel(&htim8, &sConfigOC, TIM_CHANNEL_3) != HAL_OK){
 _Error_Handler(__FILE__, __LINE__);
 }
 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
 sBreakDeadTimeConfig.DeadTime = 0;
 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim8, &sBreakDeadTimeConfig) != HAL_OK){
 _Error_Handler(__FILE__, __LINE__);
 }
 HAL_TIM_MspPostInit(&htim8);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Instm32f4xx_it.c

 #define PWM_SZ 100
 uint32_t SineLookupTable[PWM_SZ];
 const float Angle_Step_Rate=1.8;
 void waveform(void){
 uint8_t tmp;
 for(tmp=0;tmp<PWM_SZ;tmp++){
 SineLookupTable[tmp] = (TIM8_IR_CNT_VAL*(tmp+1))/PWM_SZ;
 }
 }

 void DMA2_Stream4_IRQHandler(void){
 HAL_DMA_IRQHandler(&hdma_tim8_ch3);
 }�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#timer #stm32f4 #pwm #dma #stm32f4-discovery #stm32f4-disco #stm32f4-pwm #stm32f4discovery-stm32f4 #timer-pwm
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
waclawek.jan
Super User
Posted on June 07, 2017 at 14:22

Setting repetition counter to N=nonzero will generate Update Event not upon every timer overflow, but upon every Nth timer overflow.

See RM0090, 17.4.13  TIM1&TIM8 repetition counter register (TIMx_RCR).

JW

Hobbyist
Associate II
Posted on June 07, 2017 at 15:23

Thanks for info on repetition counter.

But, How can i generate Variable PWM using

HAL_TIM_PWM_Start_DMA

160576CGIL2
Hobbyist
Associate II
Posted on May 02, 2018 at 13:44

Hi

ferrario.fabio

,

Are you able to solve issue of PWM using DMA?

Posted on May 03, 2018 at 06:57

Yes indeed thanks.

Fabio

On Wed, 2 May 2018, 13:45 Sukhdeep Singh, <st-microelectronics@jiveon.com>