cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427 USART INTERRUPT ERROR (HAL LIBRARY)

emre2
Associate
Posted on December 18, 2014 at 16:15

Hello to everyone

i have being used to std library on stm. Now i passed to Hal library. I write an Usart code. I i dont use intrerrupt its work correct. But whe i set interrupt routine its not enter to RXNE IRQ handler. Code is below could you check and help me about my mistake.

HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);

  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

  saveToFlash();

  MX_GPIO_Init();

HAL_GPIO_WritePin(GPIOH,GPIO_PIN_12,GPIO_PIN_SET);

  MX_USART3_UART_Init();

 

  

        HAL_UART_Transmit(&huart3,(uint8_t*)dene,4,1000);

  

  

while (1)

  {

   

  }

 

}

void USART3_IRQHandler(void)

{

  HAL_NVIC_ClearPendingIRQ(USART3_IRQn);

 

}

void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct;

  __PWR_CLK_ENABLE();

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 6;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

  HAL_RCC_OscConfig(&RCC_OscInitStruct);

}

/* USART3 init function */

void MX_USART3_UART_Init(void)

{

  __GPIOC_CLK_ENABLE();

__USART3_CLK_ENABLE();

  huart3.Instance = USART3;

  huart3.Init.BaudRate = 115200;

  huart3.Init.WordLength = UART_WORDLENGTH_8B;

  huart3.Init.StopBits = UART_STOPBITS_1;

  huart3.Init.Parity = UART_PARITY_NONE;

  huart3.Init.Mode = UART_MODE_TX_RX;

  huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;

  huart3.Init.OverSampling = UART_OVERSAMPLING_16;

  HAL_UART_Init(&huart3);

HAL_NVIC_SetPriority(USART3_IRQn, 0, 1);

  HAL_NVIC_EnableIRQ(USART3_IRQn);

  __HAL_UART_ENABLE_IT(&huart3,UART_IT_RXNE);

__HAL_UART_ENABLE_IT(&huart3,UART_IT_TXE);

}

Thanx.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on December 22, 2014 at 10:26

You have to use HAL_UART_Receive_IT & HAL_UART_Transmit_IT.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on December 24, 2014 at 09:56

Hi,

Please Format Code Block - Paintbrush [<>] icon, upper left of Word-in-a-box(tm) interface..

Regards,

Heisenberg.